7/10/2013 3:32 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Specially for that kind of installation is a good to have a discussion withSupport Request. There you should give an details about what exactly is restriced/removed in Winodws OS. Eventually from there to have a suggestion how to proceed. Best regards, Hristo Mihalev
|
This contribution was helpful to2 thankful Users |
7/10/2013 7:41 PM | |
Joined: 4/26/2012 Last visit: 10/17/2024 Posts: 1559 Rating: (169) |
following compatibility list. https://support.automation.siemens.com/BR/llisapi.dll?func=cslib.csinfo&lang=en&objid=9061581&caller=view |
Last edited by: rdoliveira at: 7/10/2013 7:43 PM"Always make a backup before and check the best time before testing." |
|
7/11/2013 11:05 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Check the log installation file for WINCCFLEXEXPRESS SQL Server as part from WinCC Flex instalallation:http://msdn.microsoft.com/en-us/library/ms143702(v=sql.90).aspx But really this is a shot in the dark from my side. You are right if you don't have permission to "write" the installation itself should stop with error.
|
This contribution was helpful to1 thankful Users |
7/11/2013 2:02 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (173) |
For me this sounds like a HP Notebook. If so please see following FAQ: http://support.automation.siemens.com/WW/view/en/58217334 |
Have Fun! |
|
Follow us on