7/12/2013 2:42 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello Navnag, Only a clarification,Amit_86 spoke of high frequency, this maximum is 500 HZ, I think but do not know because he has not yet explained what frequency but I think it is higher. Maybe this is better Data Sheet - Alstronthis is 100 KHz. |
This contribution was helpful to1 thankful Users |
7/12/2013 4:04 PM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating: (307) |
Thanks Ste39 I assumed a speed of a few Hz Max only as he is looking for a DI Module and not a counter module. Anyway he can choose whichever is more suitable for his application. Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
Follow us on