Industry Online Support
Technical Forum
7/14/2013 4:18 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hello Saggy It depends upon the Hardware Configuration downloaded into theCPU . ( i.eyou have download a redundant confuration in a stand alone CPU or prepared s special configuration with only 1 CPU ) If your software is written for aRedundant system and you are testing it / or providing training on it on a stand-alone system thenRedundancy fault should be present. On the othet hand if it is just a Training configuration and specific non redundant training projects are to be used then there may be no Fault indication. Some steps need to be following for using a H CPU in Stand-alone configuration. ( Pl seedetailed information - Extract from Manual ). Hope this helps Cheers Navnag AttachmentS7_400H_Standalone_Mode.pdf (265 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on