Industry Online Support
Technical Forum
10/4/2011 4:51 AM | |
Posts: 18 Rating:
|
I have following issue... I set up WinCC Web Navigator both server and client according to the manual. I want to monitor PCS7 OS via local LAN and when I connect to the main page - start page on the Web Navigator client the project is not active althought it is ok on the OS - Server PC. If I try to connect to any other page everything is ok but then I can not navigate pages like on OS. There are some pictures in attachment ilustrating this... please help urgently.... Do you have any ideas? Does it have something to do with Picture Tree Manager? AttachmentWebNavigator.pdf (179 Downloads) |
Follow us on