Industry Online Support
Technical Forum
8/3/2013 7:19 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Try with using wipout.exe. wrote: An additional possibility to reset the CPU is provided by the program "Wipeout.exe". This program is located on the Installation-CD of STEP7-Micro/WIN or is available in the Internet under Entry-ID:2123168. On the contrary to the reset via STEP7-Micro/WIN, the program "Wipeout.exe" does not only delete the user program, the data block and the configuration information, but also the baudrate is reset to 9,6 kbit/s and the netaddress is reset to address 2. The CPU is reset into the pristine status of supply. |
Follow us on