10/30/2012 1:09 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello Sudheendra; There was a discussion on the forum a few days ago on the same subject, see if the solutions proposed help you out: /tf/WW/en/Posts/80801 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/13/2013 4:16 PM | |
Joined: 8/25/2005 Last visit: 10/5/2024 Posts: 1162 Rating: (111) |
Hello JD_techflirt, with the product information of the 6ES7197-1LA04-0XA0 the information is given, that it is BASED ON IM153-BA02 and NOT FIT FOR PCS7 V6.1. Think there are the same restrictions for newer versions of PCS 7. Best regards Sabine |
This contribution was helpful to1 thankful Users |
Follow us on