8/16/2013 9:09 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hello, maybe you can change the boot.ini file on your system (on windows xp -> C:\ -> boot.ini) for Windows 7: http://windows.microsoft.com/en-us/windows7/what-happened-to-the-boot-ini-file there is a workaround if you can't find a solution: you can change the boot options (therefore go to the boot manager when your computer is starting) and set the time to 1 second. Then you only see the display for selection for only 1 second and not for a very long time.. greetings, bigfoot |
This contribution was helpful to2 thankful Users |
8/16/2013 10:58 AM | |
Posts: 148 Rating: (14) |
Totally correct only I remember that it should be 3 sec minimum value |
8/16/2013 8:11 PM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating: (29) |
How must I change the file boot.ini ? The file contains this: [boot loader] timeout=30 default=multi(0)disk(0)rdisk(0)partition(1)\WINDOWS [operating systems] multi(0)disk(0)rdisk(0)partition(1)\WINDOWS="Microsoft Windows XP Professional" /noexecute=optin /fastdetect |
"Educate the children and it won't be necessary to punish the men." |
|
8/17/2013 1:24 PM | |
Posts: 148 Rating: (14) |
change the 30 sec to 3 sec only: [boot loader] timeout=3 default=multi(0)disk(0)rdisk(0)partition(1)\WINDOWS [operating systems] multi(0)disk(0)rdisk(0)partition(1)\WINDOWS="Microsoft Windows XP Professional" /noexecute=optin /fastdetect |
This contribution was helpful to1 thankful Users |
Follow us on