8/27/2013 9:28 AM | |
Posts: 1064 Rating: (72) |
First things first are you using wincc or winccflex ? |
8/27/2013 10:01 AM | |
Posts: 61 Rating: (0) |
Sorry WinCC flexible |
8/28/2013 9:19 AM | |
Joined: 8/19/2013 Last visit: 8/8/2024 Posts: 148 Rating: (10) |
Hi gogycro, perhaps this link will help you a little bit http://support.automation.siemens.com/WW/view/de/18660846 If you want to use several/many data in your Flexible application the easiest way is to definea data block in Step 7 and then use the variables from the DB in Flex. But the other elements are possible too (memory bits, inputs or outputs) - your decision Regards |
This contribution was helpful to1 thankful Users |
Follow us on