9/1/2013 7:21 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello I noticed your post late but felt that I must reply. Of course you can Use SIPLUS RIC for S7-400H. The SIPLUS RIC Library is same for S7-400 and S7-400H. Here are the Order Nos.: 6AG6003-0BB11-0AA0 - IEC60870-5-104 PROTOCOL MASTER AND SLAVE FUNCTION BLOCK LIBRARY FOR CP 443-1 AND PN INTERFACE 6AG6003-0BA01-0AA0 - SIPLUS RIC IEC ON S7 LIBRARY RUNTIME SOFTWARE FOR AUTOMATION SYSTEM, SINGLE LICENSE FOR 1 INSTALLATION FOR REDUNDANCY STATION, IEC 60870-5-101 PROTOCOL MASTER AND SLAVE 6AG6003-0AC01-0AA0 - SIPLUS RIC IEC ON S7 LIBRARY RUNTIME SOFTWARE FOR AUTOMATION SYSTEM, SINGLE LICENSE FOR 1 INSTALLATION FOR AS REDUNDANCY STATION, PROTOCOL IEC 60870-5-103 MASTER, FUNCTION Pl see attached Extract from SIPLUS RIC Manuals regarding use in H systems. Hope this helps Cheers Navnag AttachmentSIPLUS_RIC_400H.pdf (115 Downloads) |
Last edited by: Navnag at: 9/1/2013 7:28 PMAttachment added There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on