Industry Online Support
Technical Forum
9/10/2013 5:13 PM | |
Joined: 8/22/2013 Last visit: 6/5/2021 Posts: 62 Rating: (0) |
i have a problem with the axis and drive configuration why when i define the drive message frame 999 free but in the axis indicate invalid can somebody help me? Attachmentsimotion.pdf (172 Downloads) |
9/10/2013 5:50 PM | |
Joined: 8/22/2013 Last visit: 6/5/2021 Posts: 62 Rating: (0) |
Hello, this data is invalid because the mechanism of the symbolic assigment can't read actor or sensor Interface from a undefined telegram. In the standard telegram types the interfaces are defined but telegramtype 999 doesn't supply this information. Regards Christoph sorry,the 999 telegramtype is free ,user defined,you say undefined ,i do not understand. so the message frame from the simotion.pdf axis and drive,are the same thing. i think one for communicate with axis and the other for the drive and another problem shown in the simotion.pdf thank you sir best regrards
Attachmentsimotion.pdf (157 Downloads) |
9/11/2013 1:47 AM | |
Joined: 8/22/2013 Last visit: 6/5/2021 Posts: 62 Rating: (0) |
thank you |
Follow us on