7/31/2013 4:34 PM | |
Posts: 6 Rating: (0) |
Hello All. I have a problem with newly formatted PC. I have installed PCS7 v8.0 SP1 ES and PDM on Windows 7 SP1 Prof. x64. Creating OS is facing error, When i create a project with wizard or manually into PC station. Message1 for wizard and the Message 2 for manually into the PC station. Did anybody see these messages? AttachmentOSError.zip (236 Downloads) |
7/31/2013 4:50 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hi Simatech, |
7/31/2013 5:03 PM | |
Posts: 6 Rating: (0) |
Sorry, i made mistake when writing. Its already Ultimate. |
7/31/2013 5:19 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Have you tried alreadythe procedure given by Raj_SIRIUS in the following post? |
8/1/2013 2:25 AM | |
Posts: 35 Rating: (1) |
you should connect a cable toyour network .. |
This contribution was helpful to1 thankful Users |
8/1/2013 8:58 AM | |
Posts: 6 Rating: (0) |
Yes Jumo, i have tried this. But no solution.
|
8/1/2013 12:03 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hi Simatech, to your second picture: After installing SIMATIC PDM, did you import your devices with "Device Integration Manager"? Have you tried a reimport of the device library? To the wizard message: Is the Message Queuing Service installed and Microsoft Information Service (IIS) configured? You find the description here: http://support.automation.siemens.com/WW/view/de/68157327/0/en Hope this helps. |
8/1/2013 12:16 PM | |
Posts: 6 Rating: (0) |
Hello Jumo, I do not think that problem is related to device library. This is completed anyway. Furthermore, I did not perform a Microsoft Information Server related installation. Queuing Service is already installed.
|
8/25/2013 3:19 AM | |
Posts: 2661 Rating: (279)
|
ABSOLUTELY! |
10/18/2013 2:20 PM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating: (931) |
Hello, A collegue just got the same problem. We were able to fix it by connecting the cable. I understand that Windows 7 is more intelligent then the XP version. It detects if a network is connected or not.... Some how, PCS7 checks this when inserting OS objects. Can someone tell me how PCS7 thinks? Why does it check the network configuration when inserting a OS object. I can imagine you can get trouble in netpro, but not when inserting OS objects. The error response is: CreateShare failed, no network card available... Why does this not happen when you have for example a laptop which has only one terminal bus... Does it have something to do with the CP1623 card? Or does it happen when you have more then one network card installed? Please share your thoughts.... Can't stand when PCS7 does something and dont have a explanation for it....even the so great (dutch) support group |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on