10/18/2013 10:04 AM | |
Posts: 56 Rating: (7) |
Dear Sir, I am working on projects for utility scada. In this i am using 2 PC the details are below 1. Server PC PC details :64 bit operating system, Window Server 2008 R2 standard with SP1, Resolution max 1280 x 1024, software installed :Simatic WinCC Runtime V7.0 + SP3 2. Client PC PC details :34 bit operating system, Window 7 Professional with SP1, Resolution max 1920 x 1080 software installed :Simatic WinCC Configration V7.0 + SP3 My query is i can see the scada screen properly on my client PC but at the same time the same screen i have to see with scrolling functuion means (it is not come in one screen). Please find attached two pc's installed program picture. What is the exact cause for this effect? & How can i see the all data in one screen for server pc ? What chages i need to do for the same? Kindly let me know if anything is require to resolve the issue. Regards, Ashish Wandhare AttachmentSERVER PC PROGRAM.zip (135 Downloads) |
Follow us on