11/10/2013 12:15 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
When downloading the PO objects, the CPU designation and inserted memory cards are stored.. In the case your AS crashes, and you insert the memory card in a new AS, the PO objects are not lost... The same as for a new memory card in the same AS.. When your AS crashes and your memory card is also "dead", then you lost your PO... |
If I could help you, you can use the RATE button. Thank you. |
|
11/11/2013 10:16 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Yeah I mean, When your first AS crashes and your memory card is also damaged, the PO is lost. When your first AS is crashed and you insert your memory card to a new AS, the PO is not lost because the memory card type is stored, so it will automatically recognize the PO objects. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on