9/26/2011 4:52 PM | |
Joined: 8/25/2005 Last visit: 5/15/2024 Posts: 1161 Rating: (110) |
Hello D.K, have you checked the diagnostic information of the IM 153-1 CONTROLLER? Also the dignostic buffer of the S7-400 CPU? Hope there will be some interesting information. Think everything was running befor? Have you got any information about changes, ... ? If you need urgent assistant I would start a case at the technical support (Support Request) Good luck Sabine |
9/26/2011 5:27 PM | |
Posts: 4 Rating: (0) |
Dear Mr. Sabine Thanks for reply. I am very new in this Siemens automation system. I have mechanical background and learnt the power plant electrical and control on site work. If you pl elaborate your advice and inform the procedure how to carry out this check then this will help me a lot. This is very urgent as our complete plant stop for nine days no power. Pl find attached file incident report I made and job report till date I have carried out. May be this will help to understand more our problem. Regards Dhananjay kumar pandey AttachmentMicrosoft Word - Work report on WAPCO Shagamu Break down job.pdf (159 Downloads) |
9/26/2011 5:28 PM | |
Posts: 4 Rating: (0) |
Dear Mr. Sabine Pl find attached file incident report. Regards D.K AttachmentMicrosoft Word - Incident Report SIEMENS PLC.pdf (189 Downloads) |
9/28/2011 10:25 AM | |
Joined: 8/25/2005 Last visit: 5/15/2024 Posts: 1161 Rating: (110) |
Hello D.K., no other replies so I try to be for assistance. does the problem still exist? Think it would be very interesting to have a look at the diagnostic information of the IM 153-1. We have to find the reason why this module is in stop. Please try to read out this information and post it here. Within this manual SIMATIC Distributed I/O device ET200M there are information about diagnostic information of the IM. This FAQ Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? provides information what could be done to avoid the STOP of the IM. Good luck Sabine |
11/18/2013 10:38 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to when the sinumerik boots up the keys on the controller unit panel starts flashing and it goes on for like hours Best regards O_Moderator |
Follow us on