11/22/2013 2:32 PM | |
Posts: 220 Rating: (11) |
Hi Gkarofilakis , which PCS 7 version do you use with STEP 7 and WinCC? Maybe you can lookhereif the two produkts compatible with PCS 7. |
11/22/2013 7:57 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
You cannot use seperate step7+ wincc with PCS7.. Onlysolution isto start over from scratch...ifabove statement is right that youwant to use pcs7 but have step7 +wincc installed. Dont you have to install step7 first, then wincc? Installer does the same thing... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on