Industry Online Support
Technical Forum
7/2/2013 11:27 AM | |
Posts: 43 Rating: (9) |
Dear Expert, I would appriciate if i will get voltage transformer wiring/connection diagram which is used for metering function in 3WL ACB. |
7/3/2013 5:47 AM | |
Posts: 262 Rating: (45) |
Hi dude ! As i understand you have one no of Voltage transformer MLFB/ TYPE NO. 3WL9111-0BB68-0AA0 380...690 V a.c. available with you. If you want to connect it with the Metering function module of 3WL to see the KW or voltage etc in ETU 45/ 76B you are in need of connection dig. I am attaching the relevant files which will help you to connect it with 3WL. Attachment3WL_VT Connection with BSS and Metering.pdf (380 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on