12/4/2013 6:34 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi Spet59, Have you proven the OPC client behavior being installed in the same PC that the OPC server? Is the same behavior? Check this Troubleshooting guide, maybe it helps you to find the problem if it is related with the configuration DCOM. best regards AttachmentTroubleshooting_OPC_and_DCOM.pdf (56 Downloads) |
12/10/2013 5:25 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi Spet59, Have you read this information?. I think that here is what you need : http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=44443990&load=treecontent&lang=en&siteid=cseus&aktprim=99&objaction=csview&extranet=standard&viewreg=WW best regards |
12/11/2013 2:57 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi Spet59, I found the document WinCC V7.0 SP1 WinCC Release Notes but the same as the one that appears in the url doesn't say anything of the topic, nevertheless here it is attached so that you revise it. best regards AttachmentWinCC V7.0 SP1 ReleaseNotes.pdf (32 Downloads) |
12/11/2013 3:45 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
I also attach here the manual WinCC V7.0 SP1 OPC - Open Connectivity in which appears concrete information of the topic, look the topics 10.1 to 10.2.2, and tell me if this helped you. best regards AttachmentWinCC V7.0 SP1 OPC - Open Connectivity .pdf (51 Downloads) |
Follow us on