12/6/2013 11:51 AM | |
Joined: 4/22/2010 Last visit: 10/17/2024 Posts: 5697 Rating: (715) |
Hello, Without the program hard to do Please read this: Why can't you display an STL program in FBD or in LAD? and try to split the code in multiple networks so it can be displayed in Lad. Better option, read some books about STL and leave the code as it is, changing it can influence the working of the PLC. Regards, Marcjan |
Problem solved? |
|
12/8/2013 4:51 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Hello, For more help on SFC36 , you can check "11.2 Masking Synchronous Errors with SFC 36 "MSK_FLT" " in THIS manual.System functions are part of operating system of CPU and for conversion to a new programming language for new PLC, you should seek the equivalent for the function or equivalent for the whole concept performed by it. I hope this helps youHamid Hosseini |
Last edited by: hdhosseini at: 12/8/2013 4:52 PM |
|
This contribution was helpful to1 thankful Users |
12/9/2013 11:00 AM | |
Joined: 4/22/2010 Last visit: 10/17/2024 Posts: 5697 Rating: (715) |
Hello, Look at the CX-one help for the instructionset for your type off PLC. attached you find some failure handling blocks. i don't think there is such a block in Omron. I have no experience with converting S7 to Omron, did it the other way around with much pleasure Regards, Marcjan AttachmentFal_Fals.pdf (67 Downloads) |
Problem solved? |
|
Follow us on