2/4/2008 2:51 PM | |
Posts: 5 Rating: (0) |
Hi, AttachmentDiagnostic CPU315.pdf (341 Downloads) |
2/19/2008 1:01 PM | |
Posts: 5 Rating: (0) |
Thanks for your answer, Mario. The OBs was downloaded in the plc. But now I´ve a new diagnostic file. Would you take a look on it and maybe you could say what´s wrong? Best regard Kevin AttachmentDiagnose1.pdf (253 Downloads) |
12/12/2013 12:04 PM | |
Posts: 2 Rating: (1) |
Hello every body I have the same problem with the same moudle and same Error ID as Following: Event 1 of 100: Event ID 16# 49A0 STOP caused by parameter assignment error or unpermissible difference between preset and actual configuration: startup disabled No relevance for user (SDB no.): 5 No relevance for user (Z2): 0000 (Z3): 000f Previous operating mode: STARTUP (warm restart) Requested operating mode: STOP (internal) External error, Incoming event But my system is consists of two CPU as Redundancy, each unit icludes: S7 315-2 DP CPU, CP342-5 and IM153-2 . They are connected through MPI for CPU's and OP77B panel, Profibus for DP (IM's) the first CPU is working but the second is OFF with the error as mensioned above, SF LED is lit, STOP LED is lit , OP panel is ON with no display on the screen. Please Help to figure out what is the problem and don't hesitate to ask for further information . thank you very much.
AttachmentModule Information.pdf (235 Downloads) |
Last edited by: Ojali at: 12/12/2013 12:07 PM |
|
Follow us on