12/16/2013 6:18 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hi Pej, try to look at this if it can help you: http://support.automation.siemens.com/WW/view/en/16532946 |
Last edited by: Ste39 at: 12/16/2013 6:20 AM |
|
12/17/2013 2:43 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Pej, This adapter also works for S7-200, be careful because I think that if you have very old CPU S7-200 does not work. Which configuration do you need for "PC Adapter USB" in conjunction with MicroWin and S7-200? |
12/20/2013 11:37 AM | |
Joined: 1/9/2013 Last visit: 2/5/2022 Posts: 9 Rating:
|
Hello, The type of the CPU is 214-1AD23-0XB0 the Version of the Microwin is V4.0.9.25( Microwin V4 sp9) . in the attached file you will see the picture of errors when I am trying to connect. the first one is the error when I am choosing PC-Adapter Auto(PC-adapter Auto1) in PG/PC interface option. The second one is the error when I am choosing the PC-Adapter PPI ( Adapter PPI1) in PG/PC interface option. it will be in the next message. The configuration of the PPI option is also in the picture in the next message Attachmentpcadapter Auto1.pdf (76 Downloads) |
12/20/2013 11:41 AM | |
Joined: 1/9/2013 Last visit: 2/5/2022 Posts: 9 Rating:
|
here is the error for PPI in PG/PC interface
Attachmentadapter ppi.pdf (84 Downloads) |
12/20/2013 12:52 PM | |
Joined: 1/9/2013 Last visit: 2/5/2022 Posts: 9 Rating:
|
the configuration of the PPI interface
Attachmentpc adapter ppi.pdf (74 Downloads) |
Follow us on