Industry Online Support
Technical Forum
12/29/2013 11:37 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, Have a look to the annex. You will see that in the simatic Net menu there is a symbolic editor. The editor has a help file explaining how to work with it. You can export/import files in the editor. A way to know the structure of the export/import file is to create a short sample. You export the sample, and than you add your own symbols, and import again. Once you have symbol file, you have to specify via the menu "communication settings" that you want to use it. First stop the OPC server via the menu. Add the symbol file to the settings, restart the OPC server. Have also a look to the "gettimng started", chapter 4.4 and 4.5 http://support.automation.siemens.com/WW/view/en/77377601 Attachmentopc.pdf (377 Downloads) |
Last edited by: jklm at: 12/29/2013 11:41 AMBest regards |
|
Follow us on