1/8/2014 12:53 PM | |
Posts: 27 Rating: (14) |
I'm a little confused , the module CP 342-2 (6GK7 342-2AH00-0XA0). is an ASi-master CP module but in your message you refer to profibus not working. If it is the ASi cp attached is a table of faults which are indicated by the module leds In OB82 M38.4 is set high when a fault is signalled by the module with diagnostic address 272 , this bit is then reset when the fault is cleared AttachmentCP342_ErrorIndicators.pdf (86 Downloads) |
Last edited by: Brynboy17 at: 1/8/2014 1:04 PM |
|
Follow us on