Industry Online Support
Technical Forum
2/17/2014 1:29 PM | |
Joined: 3/3/2011 Last visit: 12/28/2021 Posts: 81 Rating: (10) |
Hi! When I try to use WinCC Configuration tool, after I have made OS Project Editor settings, I got a lot of error related to System Messages. -Not all limit value monitoring could be generated! When i open the Reading error sheet i have a list with the same "Table type" and "Error text". The table type is relate to the "Single message table" and the Error text is "The set message class or message type does not exist!". Almost every system messages. In Message bloks and Message categories table in names colums there are "0" instead of name of the object. I attach an excel according to a new empty project. I use WinCC 7.0 SP3, on Win 7 Prof Eng. Does anybody have a solution to this issue. Thank you: Labirex AttachmentEmty_Proj_Excel.zip (59 Downloads) |
Follow us on