10/13/2011 10:03 PM | |
Joined: 5/29/2007 Last visit: 11/23/2023 Posts: 28 Rating: (0) |
Hello! I have a problem like the probleminthis link , but in the reverse order. In my case AK 1703 ACP is Profibus DP Master and CPU314-DP slave. Sycon software for Profibus says that S7-300 isn't configured properly like slave. how canI do this? Thank You in advance |
10/13/2011 10:29 PM | |
Joined: 9/27/2006 Last visit: 5/28/2024 Posts: 12257 Rating: (2668) |
Hello valparaiso; This is a situation similar to connecting a S7 CPU as a DP-slave to a S7 DP-master in a different project. Look at the following FAQ and follow the instructions to setup the CPU as a DP-slave: http://support.automation.siemens.com/WW/view/en/19449428 Then configure the data exchange areas in the slave as required. As a test, use the data exchange as proposed in the example, if you wish. Download the HWConfig to the S7-314-2DP. Import the gsd file for the S7-314-2DP in Sycon (the gsd file is found in a link provided in the FAQ). Insert the S7-314-2DP slave in the Sycon Profibus network, and set up the data exchange based on the areas selected in the slave, but in reverse (a Input areain the slave configurationbecomes an output from the master, the size must remain the same). Again as a test use the data exchange proposed in the FAQ for the master. Download the Sycon configuration to your DP-master. Connect the master to the slave, and if everything has been configured correctly, you should have communications between the two. If there is a problem, try opening the diagnostic buffer on the slave CPU to see what it doesn'tlike; I believe Sycon han an Online mode that can help diagnose your master too. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/13/2011 10:33 PM |
|
10/13/2011 10:59 PM | |
Joined: 5/29/2007 Last visit: 11/23/2023 Posts: 28 Rating: (0) |
Thank you, dchartier! I will try your advice in Monday, when i'm back to work. Best regards |
10/19/2011 4:19 PM | |
Joined: 5/29/2007 Last visit: 11/23/2023 Posts: 28 Rating: (0) |
Some images from Properties DP in Hardware Config (step 7 - cpu 314d-2dp slave dp)AttachmentProperties DP.zip (129 Downloads) |
5/24/2012 4:24 PM | |
Joined: 5/29/2007 Last visit: 11/23/2023 Posts: 28 Rating: (0) |
Thank you Mike J |
2/20/2014 11:07 AM | |
Posts: 340 Rating: (6) |
new question is splittet to no commnunication, DP Master is TM-1703 and CPU315-2DP is slave |
Follow us on