Industry Online Support
Technical Forum
2/27/2014 4:14 AM | |
Joined: 8/25/2006 Last visit: 4/29/2024 Posts: 2203 Rating: (277)
|
Hello. You need to connect your PG/PC directly to the local CPU interface (X01 in PM6), because when communication error is active other interfaces may not work (CS7/SS4). Try the latest version ofIBS. Check COM-port settings. Try to do the following: 1. Start IBS, then menu 'Activities-IBS Program'. 2. Then menu 'Diagnostics-Start Debug Monitor', enter CPU number. 3. Then menu 'Service-Exit IBS Program'. 4. Then menu 'Activities-HEX/Debug Monitor'.
|
Follow us on