3/15/2014 12:06 PM | |
Joined: 6/1/2010 Last visit: 7/9/2024 Posts: 160 Rating:
|
Dear Expert, We have belt conveyors for raw material and to protect them we use ZSS PROXIMITY switch [ZSS-zero speed sense] at belt end. If motor is ON and in this condition is it belt also moving[or elsemotor and belt mechanical arrangement is disturbed.] [ZSS fixed at conveyor to sense striker plates to generate pulse]. So if after Motor is ON and ZSS signal is unable to achive at PLC till 20sec then it will TRIP motor to stopconveyor and its series. We Need : Instead of this ZSS unit is it there another technic available ? or is it instead of this ZSScan use other instruments ? ( ZSS : --> Type IPS D3 OG NO , 10-30 V DC,PNP,200mA) AttachmentC:\Documents and Settings\11223\Desktop\ZSS.zip (79 Downloads) |
Last edited by: A9K at: 3/15/2014 12:09 PMLast edited by: A9K at: 3/15/2014 12:08 PMA9K |
|
3/16/2014 9:25 AM | |
Posts: 8946 Rating:
|
First of all, here is a master - link: Proximity switches all over the world: http://lmgtfy.com/?q=proximity+switch#seen Than also here you will find all kind of proximity sensors: http://www.pepperl-fuchs.com/global/en/classid_143.htm http://www.automation.siemens.com/simatic-sensors-static/ftp/e20001-a120-p872-x-7600.pdf http://www.ifm.com/ifmgb/web/ps/select010_010_020.html ifm is very popular in germany and has high quality. |
3/16/2014 11:46 AM | |
Posts: 8946 Rating:
|
You are welcome! Nice holidays also! |
Follow us on