Industry Online Support
Technical Forum
3/17/2014 9:52 AM | |
Posts: 17 Rating: (0) |
Iam posting this again expecting any answers , Please help out Dear Friends ,
Iam trying out and trying out to solve the problem , But cannot solve it i hope here the problem could be solve , Iam using Analog IO module SM 1234 , Im using the Scaling Blocks NORM_X and then SCALE_X , but my main problem is I have configure the Analog Module to terminal 2+ & 2- where it represents IW100 , Iam using fluke injector when iam injecting on this terminal my value is not increasing , I have attach some screens shots in steps : screen shot 1 : shows the module , screen shot 2 :shows where iam injecting with two probes on terminal 2+ & 2 - , screen shot 3 : shows the multimeter after touching the probes to the terminal as shown in screen shot 2 still in the screen shot 3 their is nothing even i press the min and max button shown on the injector no value its all shows as --.---- , screen shot 4 shows the block of NORM_X where after pressing the min and max button on injector still the value on IW100 is 0 (zero) , screen shot 5 is the configured module, where as screen shot 6 : is the channel 2 , IW 100 and measurement type is selected to 0-20mA , everything i have done but still when i place the probes on the terminals of 2+ & 2- nothing is working as all screen shots shows , Is anything missing or something gone wrong, kindly please help me out , Thanks waiting for your reply please please please . may be my way to represent is confusing kindly apologize . thanks AttachmentSCREEN SHOT 1,2 ,3 ,4 ,5 , 6 .pdf (67 Downloads) |
3/17/2014 10:08 AM | |
Posts: 340 Rating: (6) |
closed cause question posted twice. The second thread with the subject PROBLEM WITH ANALOG INPUT SM1234 AI/AQis published within the same conference. |
Follow us on