Industry Online Support
Technical Forum
3/14/2014 1:27 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, Copy Ram to Rom is not supported by the S7-400, read more here: What is the effect of the STEP 7 function "Copy RAM to ROM"? Download to memory card works, but CPU goes in stop, that's why it's often forgotten after small changes in program. How can you write the program to the FLASH Memory Card when using a SIMATIC S7-400 CPU? Regards, Marcjan |
Last edited by: Marcjan at: 3/14/2014 1:30 PMProblem solved? |
|
This contribution was helpful to
4 thankful Users |
3/18/2014 5:06 PM | |
Posts: 25 Rating:
|
i only refer to offline help on step 7, thus i thought copy ram to rom was also functioning for s7-400 since it is also highlighted when i select menu>PLC.. it is great to have this forum and people like you Marcjan. thank you very much. also i am glad you have included the link it really helped a lot. |
This contribution was helpful to
2 thankful Users |
Follow us on