8/2/2012 4:18 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating:
|
Hello S7Mgr, you need a GSD file to import the drive in HW Config. After the GSD file import, you will find the drive under "other field devices" in the HW catalouge. You will have to read the manual of the Lenze drive to find out how control word and setpoint have to be and if it requires further values from the PLC. Without knowing any Lenze drive I say: To parametrate the drive you will need a software from Lenze or a operator panel (I don't know if there is one) or you have to do it directly on the drive. Go to http://www.lenze.com/en/home/and look for a manual, a GSD file and if there isa parametrating software. |
|
|
8/2/2012 6:11 PM | |
Joined: 1/22/2008 Last visit: 2/10/2022 Posts: 77 Rating:
|
Hi, Quick question: Can I use USB MPI adapter to download program from GDC to drive. Regards, |
8/3/2012 10:27 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating:
|
Hello, To clarify the things because there are two points: 1. In Step7 need to make configuration in order to assign that drive (corresponding GSD filehttp://akb.lenze.de/akb-englisch/infopool.nsf/HTML/200412329) will be connected via Profibus to CPU (address:X) and will exchange Y number of words. 2. Configuration of all above mentioned settings in Lenze drive. Both informations should correspond 100% in order to have 'good' communication. These points are in order to establish communications. Meanwhile that drive with its coupled motor/s should be commissioned (optimized). For that you need either software or drive operator panel (as maimi said). Almost all type of drives have a panel which helps for input parameters, of course using manual (you can find it in google)?In case you are using software (GDC) I don't know if USB/MPI cable will not work together in order to be online with drive (there is mentioned:
You can try it. Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
3/20/2014 6:35 PM | |
Posts: 29 Rating:
|
That part number is from now obsolete Lenze 9300 servo inverter. The current model is 9400. http://www.ctiautomation.net/Lenze-9400-Servo-Drives.htm |
Follow us on