8/24/2013 3:20 PM | |
Joined: 9/27/2006 Last visit: 5/22/2024 Posts: 12257 Rating: (2668) |
Hello AMOL; What network do you think you would use, Industrial Ethernet or Profibus-DP, Siemens offers fiber solutions for both: Ethernet: SIMATIC NET Twisted-Pair and Fiber-Optic Networks SIMATIC NET PROFIBUS Optical Link Module OLM / P11 V4.0 OLM / P12 V4.0 OLM / P22 V4.0 OLM / P11 V4.0 OLM / G12 V4.0 OLM / G22 V4.0 OLM / G12-EEC V4.0 OLM / G11-1300 V4.0 OLM / G12-1300 V4.0 Operating Instructions
S Glass FOC: multimode (MM); 100BASE-FX BFOC
2 BFOC sockets per port, data rate 100 Mbps, for connection of multimode FOC in environments with high EMI levels and for distances up to 3000 m between two OSMs
S Glass FOC: single mode (SM); 100BASE-FX BFOC
2 BFOC sockets per port, data rate 100 Mbps, for connection of single mode FOC in environments with high EMI levels and for distances up to 26 km between two OSM ITP62-LD modules Hope this helps, |
9/3/2013 1:01 PM | |||
Joined: 9/27/2006 Last visit: 5/22/2024 Posts: 12257 Rating: (2668) |
Hello Amol; Chapter 7 of the Profibus networks manual gives details for the F.O.glass cable and connectors (to connect to an OLM) that you would require: PROFIBUS Networks - Siemens Glass fiber, standard cable: 6XV1820-5ah10: chapter 7.3.1 and table 7.4
Which connector do you use to connect fiber-optic cables to the optical interface of network components and terminals? Hope this helps,
|
||
4/2/2014 10:10 AM | |
Posts: 47 Rating: (7) |
hi amol 6GK1820 not adequate for use it in underground or so There are ruggedGlass Fiber Cable with 4,8, or 12 fibers available. A-DQ(ZN)B2Y The ends will be connected to optical distribution frame. It has standard ST Connectors for BFOC plugs. In the cabinet standart optic patch cable can be used. Or 6GK1820 when lead to somewhere outside cabinet but indoors,in the raceway ect. e.g. http://www.hitechcontrols.com/cables/data_network_bus/helucom_fiber_optics/buffered_outdoor_maxi_adqznb2y.html Best regards hela |
This contribution was helpful to1 thankful Users |
Follow us on