7/2/2009 9:57 PM | |
Joined: 1/29/2006 Last visit: 4/23/2024 Posts: 446 Rating: (64) |
Hey, NewTech I propose using of FB instead of FC and use of IEC timers in instances.Printout of this new FB is attached. You can use this FB in your program as many times, as you want (of course, each time with different instance!) and it is completely without absolute addressing....... Complete example project follows..... (there is only 1 attachment allowed with 1 post??) Have fun! uel123 AttachmentMonitoring change FB351.pdf (172 Downloads) |
This contribution was helpful to1 thankful Users |
7/2/2009 9:59 PM | |
Joined: 1/29/2006 Last visit: 4/23/2024 Posts: 446 Rating: (64) |
..... and your changed project: have fun! uel123 AttachmentComm_tes_V2.zip (141 Downloads) |
4/10/2014 1:56 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
follow up question published by jruzis split to a seperate thread with the subject Positive Edge doesn't work anymore?. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on