Industry Online Support
Technical Forum
4/28/2014 7:17 PM | |
Joined: 7/7/2010 Last visit: 6/6/2024 Posts: 14771 Rating: (2378)
|
The freqvency converter is HW address 283. And the maintenance LED is ON. If I remove the freqvency converter out of project and download the hardware with V13, then CPU seems to be normal and running. If I do the same hardware configuration with TiaPortal V12, everything works and there are no errors or maintenance led. What has changed in TiaPortal V13??? Can anyone give help? Thanks! MPJR It may be possible your V13 installation has an installation in need of repair. It may be possible V12 tolerates a profinet error that V13 does not, like something with a device name not matching - no spaces, no Unicode only characters. My suggestion for this type of problem is to report it to Siemens via Support Requestso they can address it, patch it, and make it available to everyone. |
science guy |
|
Follow us on