5/22/2014 10:20 AM | |
Joined: 11/8/2005 Last visit: 2/15/2024 Posts: 335 Rating: (3) |
How can I stop motor in PCS7 from faceplate in local mode? |
Last edited by: SM at: 5/22/2014 10:20 AM |
|
5/22/2014 10:42 AM | |
Posts: 220 Rating: (11) |
Hi, in following thread you should find an answer. Good luck
|
5/22/2014 11:37 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
HiSM Could you please express your request with more details. As mentioned in the motor block attached help:
AttachmentLocal mode.pdf (184 Downloads) |
Best Regards |
|
This contribution was helpful to1 thankful Users |
5/22/2014 1:27 PM | |
Joined: 4/8/2013 Last visit: 4/18/2024 Posts: 95 Rating: (7) |
as stated you should not control the device when in local mode because it is being controlled by another system. what you can do however is connect some block to your motS that will take it out of local mode, then perform you actions and then put it back into local mode again. (this ill only work if you "local" plc system is synced with your current system) |
5/22/2014 1:55 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello SM, as Khaled_Ezzat Mention you have to Setup the Parameter Based on the File Attached also in the APL V8.0 SP1 Manual Page no. 894 you have a Connection List. You have to Play with "LocalLi" "LocalOp*" & "LocalSetting" setting What you have to set you will find on Page no. 67. or tell you Detail Operation about the motor So we will tell you the Setting. |
Ammy |
|
This contribution was helpful to1 thankful Users |
Follow us on