5/27/2014 2:14 PM | |
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating: (12) |
Hi, Please use below link of manual: https://cache.automation.siemens.com/dnl_iis/Dg/Dg2NjI5AAAA_36195862_HB/ps7tsy_b_en-US.pdf It has explained all the possible way of time synchronisation for the PCS7 plant. |
Regards, |
|
This contribution was helpful to2 thankful Users |
5/27/2014 5:39 PM | |
Joined: 4/8/2013 Last visit: 4/18/2024 Posts: 95 Rating: (7) |
as i looked into the SiClck product it seems it has optionsfor related stations to have the "SICLOCK reception Service" installed to interface with the physical SiClck device. http://support.automation.siemens.com/WW/view/en/63288473/133300contains all the SIClck manuals since i dont know which version esactly you use. for PLC's http://support.automation.siemens.com/WW/view/en/75289704contains a section of using a central clock unit and for PC's aswell http://support.automation.siemens.com/WW/view/en/76814165 Depending on thereliability you can choose this system to sync just one system and let the rest up to the PCS7 time sync within PCS7 as in the link posted by RJ |
Follow us on