5/30/2014 2:31 PM |
|
Posts: 39 Rating: (9) |
DearEr.digu As In adddition the neutral point of anelectrical supplysystem is often connected to earthground,ground and neutralare closely related. Under certain conditions, aconductorused to connect to a system neutral is also used for grounding (earthing) of equipment and structures. Current carried on a grounding conductor can result in objectionable or dangerousvoltagesappearing on equipmentenclosures, so the installation of grounding conductors and neutral conductors is carefully defined in electrical regulations. Where a neutral conductor is used also to connect equipment enclosures to earth, care must be taken that the neutral conductor never rises to a high voltage with respect to local ground. |
5/30/2014 3:21 PM |
|
Posts: 202 Rating: (16) |
hi there can you tell me where is the neutral created that us at the alternator end or at the power transformer end???? |
5/31/2014 8:36 AM |
|
Posts: 73 Rating: (6) |
Hi, AttachmentD:\Manual Collection\PCS7 Compendium_V80\english\pcs7_compendium_part_e_en-US_en-US.pdf (281 Downloads) |
Last edited by: Krrish !! at: 5/31/2014 8:40 AM |
|
Follow us on