Industry Online Support
Technical Forum
5/22/2014 11:24 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
SatecPM130EH have different options. I suggest you to choose the option with Ethernet, Profibus or RS-232 to be sure, that connection with PG will work. Any of these interfaces present in PG M2. However, the MPI/DP port located in the PG is an RS-485 port from electrical point of view, so feel free to try this type of connection. Just read SATEC manual locatedherecarefully.
|
5/22/2014 11:53 AM |
|
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (23) |
You can use that port as RS 485. |
5/31/2014 1:40 PM |
|
Posts: 59 Rating: (1) |
RS-485 Connectivity is Possible If any Modbus Supported Device And It Check by 232 to 485 Convertor with PC in Modbus View Software REgard shailesh |
Follow us on