5/23/2014 9:40 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! Basically, all the information you need during of installation of automation systems located in simatic module data manual and installation manual for CPUs (example). However, if you are looking for more specific information or just want to know the general earthing/grounding principles in low-voltage installations and/or building installations use these standarts: 1.IEC 61131 (Part 2) - General standard for PLCs 2.IEC 60364Electrical Installations for Buildings 3.IEC 61800 Adjustable speed electrical power drive systems List of IEC standards (actually incomplete, but large enought) locatedhere. If you have specific question - feel free to ask) |
This contribution was helpful to1 thankful Users |
5/23/2014 10:46 AM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326)
|
You should not do it like it was done in the picture! |
|
|
This contribution was helpful to4 thankful Users |
5/24/2014 12:07 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello IBN-Service Most of the new Installation guidelines have a small section about "Equipotential Bonding" without providing a comprehensive Earthing Guideline, which to my mind is a very important part of installation. You are perfectly right in saying that the Drives manuals generally give better description. The best description that I could locate in is the attached manual for Motion Control ( Page-21 ) In fact, the old SIMATIC-S5 manuals always had very detailed guidelines regarding Earthing, and EMC protection. I wish, Siemens provides a Comprehensive set of guidelines to users as this is one critical area where users are most ignorant. Cheers Navnag AttachmentEMC_installation_guidelines_basic_System_Requirements.pdf (1474 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
5/26/2014 12:38 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Nice manual, thanks! |
This contribution was helpful to1 thankful Users |
6/1/2014 9:13 PM |
|
Posts: 114 Rating: (12) |
i hope this may help u /tf/WW/en/postattachments/download?attachmentId=45786
|
Follow us on