6/24/2010 11:24 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Pieter, Try to do this in Printer settings. Best regards, Hristo Mihalev |
6/24/2010 12:30 PM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Dearpie_vd, Configure in the printer settings. I did the same way in my project and it is working fine.
|
_______________________________________________________________ |
|
6/2/2014 4:32 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
HiRaviS In this case try to use a pre-configured layout nad set a print job to it.
|
Best Regards |
|
This contribution was helpful to1 thankful Users |
6/2/2014 5:12 PM | |
Posts: 559 Rating: (87) |
To do the settings in printer from the control panel is the best option. |
Follow us on