Industry Online Support
Technical Forum
9/27/2007 8:38 AM | |
Posts: 2930 Rating: (432) |
Hi, if you want ot use a Profibus connection then you need a 215 or the EM277. But you can use a MPI connetion. So S7-300/400 PLC can read/write data from/to a S7-200 PLC. Max. baud rate is 187.5kbs. Here more inforamtions: http://support.automation.siemens.com/WW/view/en/747743 I hope this helps. helmut |
9/27/2007 8:52 AM | |
Posts: 13 Rating: (0) |
Helmut, I try to connect on MPI S7-300 to S7-200 and I can't. Can oyu give me an project with hardware configured? Thank you anyway, Razvan |
Follow us on