6/1/2014 3:43 PM | |
Posts: 6 Rating: (0) |
Please could some help me ? I will return to the site tomorrow morning without any internet acces and i don't know how to solve my problem. Best regards. |
6/1/2014 4:46 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
HelloMohcine, Unfortunately, moderators haven't moved your post to PCS7 conference yet. I believe you would get more help in PCS7 conference (Don't know if it's appropriate to create a new thread in there and later on moderators will compile the 2 threads together). [quote user="Mohcine"]I'm using the following software and hardware: - ......... - DI CARD 326-1BK01-0AB0 I have some other cards (DO, AI, AO) but i made a program test to understand the problem. I'm not using the cards on F system but on normal mode. ..... ..... Do you have other modules working redundantly?!With this configuration the compilation and download is ok but physically the system is not working: - All my drivers CH_DI are on QBAD mode. - On the corresponding OR_M32_C blocks, ACTIVE_L and ACTIVE_H values are 0 (module not active). - On the hardware diagnostic view, they are no error displayed.. Can you try redundant IOs without the the module 326-1BK01-0AB0? Can you disable all diagnostics of this module (326-1BK01-0AB0) and test redundancy? I wish if I can help you more but I don't have enough experience with redundant IOs PCS7. I don't know if you ever readthis documentbut maybe you can find something between the lines. Last but not least, my PCS7 colleague had a problem with redundant IOs in PCS7 couple of weeks ago and contacted Siemens support and the problem was solved quickly. Maybe you can give it a try with hotline when you are in site. Best regards, H-H
|
Follow us on