Industry Online Support
Technical Forum
9/27/2007 7:36 PM | |
Posts: 18 Rating:
|
I'm using WinCC DataMonitor V6.2 in a PC with XPproSP2 with all updates, WinCC V6.2 with its project and Step7. In the WebPage of DataMonitor if I try to open Excel Workbooks or Published Reportsa pageappears with the error in "msg_1" file, this using the IE in the same PC with DataMonitor Server If I try using IE in another PC the error issimilar but not the same..... Can someone help me? Attachmentmsg_1.pdf (202 Downloads) |
Follow us on