Industry Online Support
Technical Forum
9/28/2007 2:29 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hi About migrating (conversion) my solution and advaice is to start build program again in Step 7. The versionofStep7doesn't metter, if this is your first question. If you readmanualaboutS5-S7( attachment)you'llseethatsomeoffunctionofstep5dosn'thaveanaloginstep7.Andifyoumake somehowtheconversion, must check everything this includes the logic of the program. May be the faster way is to start new program with logic from the S5 program. And the other thing you can convert only in Step 7 (CPU 300 and 400) not in Microwin (CPU 200) Best regards umencho Attachments7_s5s7b.pdf (253 Downloads) |
Follow us on