6/3/2014 12:00 PM | |||||||||||||||||||||
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating: (797)
|
Hello, for asynchronous Motor there is no torque and voltage constant. Some data you find Configuration Manual. http://support.automation.siemens.com/WW/view/en/46484744 Starter has motordata of standart siemens motors.
|
||||||||||||||||||||
With best regards, |
|||||||||||||||||||||
6/12/2014 4:15 AM | |
Joined: 2/25/2014 Last visit: 6/17/2024 Posts: 61 Rating: (4) |
Q1. whichwinding resistancedo I select,stator or rotor resistance? 1.winding resistance [ohm], winding resistance = (in 1PH8 asynchrous motor case) Q2. How to calculate damping coefficient, Torque Constant, and Voltage Constantin detail? 1. damping coefficient [Nm/rad/sec] 2. Torque constant [Nm/A] Torque constant = rated Torque / rated current ? 3. Voltage Constant [V/1000rpm] Voltage constant = rated voltage / 1000rpm ? Q3. aren't there torque constant, voltage constant, and damping coefficient in induction motor(asynchronous motor)? and Why doesn't it exist in? It supposed tocalcurat torque constantIn servomotor case. Approximately Rated torque / Rated current AttachmentC:\Users\sel05113\Desktop\Projektierungsdaten_1FK7022_76[1].pdf (263 Downloads) |
Last edited by: dokyunko at: 6/12/2014 4:21 AMLast edited by: dokyunko at: 6/12/2014 4:19 AMLast edited by: dokyunko at: 6/12/2014 4:16 AM |
|
6/18/2014 2:50 AM | |||||||||||||||||||||
Joined: 2/25/2014 Last visit: 6/17/2024 Posts: 61 Rating: (4) |
Q1. whichwinding resistancedo I select,stator or rotor resistance? 1.winding resistance [ohm], winding resistance = (in 1PH8 asynchrous motor case) Q2. How to calculate damping coefficient, Torque Constant, and Voltage Constantin detail? 1. damping coefficient [Nm/rad/sec] 2. Torque constant [Nm/A] Torque constant = rated Torque / rated current ? 3. Voltage Constant [V/1000rpm] Voltage constant = rated voltage / 1000rpm ? Q3. aren't there torque constant, voltage constant, and damping coefficient in induction motor(asynchronous motor)? and Why doesn't it exist in? It supposed tocalcurat torque constantIn servomotor case. Approximately Rated torque / Rated current ----------------------------------------------------------------------------------------------------------------------
AttachmentC:\Users\sel05113\Desktop\Projektierungsdaten_1FK7022_76[1].pdf (265 Downloads) |
||||||||||||||||||||
Last edited by: dokyunko at: 6/18/2014 2:51 AM |
|||||||||||||||||||||
6/18/2014 8:57 AM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Hello, following the definitions of the motordata`s: http://support.automation.siemens.com/WW/view/en/79690594 Zako |
Follow us on