6/26/2014 10:06 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hellolittle_tiger Marcjanis absolutely right !! Here is the link of the original FAQ : Maybe you can request your supplier to replace it with the correct EPROM/EEPROM. Cheers Navnag
|
There is no such thing as the last bug in a program |
|
6/26/2014 11:35 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello little_tiger Following EPROMS / EEPROMS are released for use with S5 95U 6ES5 095 8MD03 / 8MD03 Memory submodule (EPROM) 8 Kbytes 6ES5 375-1LA15 Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
6/27/2014 11:52 AM | |
Posts: 17 Rating: (0) |
Anybody have the catalog for the EEPROM 6ES5 375-0LC61? |
7/1/2014 10:33 AM | |
Posts: 17 Rating: (0) |
I have two different type of PLC. CPU 6ES5095-8MA01 and CPU 6ES5095-8MD03 Both also choose this EPROMMemory submodule (EPROM) 32 Kbytes 6ES5 375-1LA41, is it ok? |
Follow us on