6/11/2014 11:16 AM | |
Posts: 567 Rating: (107) |
As I know the status of batch server have to be "Running"!. You can find this information also in the SIMATIC BATCH Manual under chapter 8.1.2 "Starting BatchCC" under point requirement. "...To start BatchCC or the BATCH Recipe Editor, the BATCH Launch Coordinator must be started and the "Running" status must be displayed in the information bar...." |
6/11/2014 11:25 AM | |
Posts: 27 Rating: (0) |
The Launch coordinator is already running, and the batch project started in manual mode. |
6/11/2014 12:32 PM | |
Posts: 567 Rating: (107) |
Did you have a valid IP addressfor the terminal bus ethernet connection? |
7/18/2014 9:11 AM | |
Posts: 1 Rating: (0) |
I am also facing the same issue. |
Follow us on