Industry Online Support
Technical Forum
8/11/2014 10:52 AM | |
Joined: 10/11/2006 Last visit: 9/2/2024 Posts: 5902 Rating:
|
Hello, for motor dimensioning you need some more details like: - load inertia - load cycle (speed/sec.) With that you can calculate the required torque. If your listet torque of 28,25Nm includes the load inertia you have also to consider the speed. Switch rotation up to twice a second is usually not the problem. You can use the tool SIZER for complete dimensioning like motor but also converter. Link: http://support.automation.siemens.com/WW/view/de/54992004 You could consider the motor type 1FK7 / 1FT7 for your application. |
With best regards, |
|
Follow us on