Industry Online Support
Technical Forum
8/13/2014 9:16 PM | |
Posts: 6 Rating: (0) |
Sir I want to control voltage in an 12V electromagnet. A displacement sensor delivers corresponding voltage for different displacement. PLC input takes this and sends the output signal according this input. If sensor sends high voltage then PLC input voltage will be increased but output voltage should be decreased and Vice-versa is happining if sensor sends low voltage. I need a ladder diagram for this type of control. I also need PID or PD controlling for megnetic levitation a Iron bar. Please sir help me..............Please . This is my modle
Attachmentmethodology2.pdf (170 Downloads) |
8/13/2014 9:33 PM | |
Posts: 5225 Rating: (1191) |
..unintentional double posting.. See also: [LINK] |
8/14/2014 8:15 AM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is also published in the following thread want a ladder diagram. Best regards O_Moderator |
Follow us on