Industry Online Support
Technical Forum
9/4/2014 3:51 PM | |
Joined: 7/7/2010 Last visit: 6/7/2024 Posts: 14771 Rating: (2378)
|
If you have your image on a screen and drag the screen over between V13 to V11 project (with both running at the same time right?), does the image transfer with the screen, or just a placeholder for the image? Do you not have the original image? Since what you seem to care about the most is an image, why not use a screen capture program to snag the image with it open in V13, save, and then add to your v11 project. This is not the preferred way, but if this is the only thing keeping you from making progress on your v11 project, this approach will certainly work. Now, I have to wonder if the image you are trying to copy is copy protected and perhaps a built in library image that is not part of v11, so does not transfer. If you are still looking for an alternative for the generic question for transferring global libraries *down* in Portal Versions, please contact Support Requestand report back any suggestions or tools they provide. |
science guy |
|
Follow us on