Industry Online Support
Technical Forum
9/20/2014 2:26 PM | |
Joined: 4/8/2009 Last visit: 2/7/2024 Posts: 83 Rating: (1) |
Dear All, My Project Have following configuration 1st H station (AS Forming) Details:- CPU 417-4H with CP443-1 2nd H station (Simativ H Conveyors) Details:- CPU 414-4H with CP443-1 Wincc Station:- OS1 as ESOS with reduntant CP 1623 cards Wincc Station:- OS2 as OS with reduntant CP 1623 cards Both H station are used as FH. Both H-Stations are configured under Fail safe. Please refer Attachment of Netpro Configuration. OS1 and OS2 Accessing Both H-station Tags under two Named connections. This named connections is configured in Netpro as S7-fault tolerant connections. Both H Stations also communicating each other through S7-Fault tolerant connections. Now 1st H station and WinCC stations communication has established. But 2nd H stations communicates either with Wincc stations(OS1 & OS2) or with 1st H stations. means 2nd H stations to wincc stations(OS1 & OS2) and 2nd H station to 1st H-station communicationnot establishing simultaniously. Please give me solution to establish communications simulateniously.... what could be the problem...?? AttachmentNetpro Config.zip (76 Downloads) |
Follow us on