Industry Online Support
Technical Forum
10/17/2014 3:58 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359)
|
Hello wharjm01, It is really easy to understand if you read the online manual and find out the concept behind these functions FC16(I_STRING) from IEC library and FC95(HTA) from TI-S7 converting blocks . For a more practical discussion please read "Represent INT in HEX" very carefully.Despite the fact that the samples are in SCL,You can apply them in LAD and snapshots of results in each case will help you a lot.
This is up to you to select one, change you input value (in hex or decimal mode) and convert.In case of STRING processing(the next step), you should provide more information for more constructive suggestions. I hope this helps, Hamid Hosseini |
Last edited by: hdhosseini at: 10/17/2014 4:34 PMLast edited by: hdhosseini at: 10/17/2014 4:02 PM |
|
10/17/2014 4:06 PM | |
Posts: 79 Rating: (1) |
make sure you string length is adquate. rememeber the first two bytes of the string are used by the system for string length and actual data in the string. |
Follow us on